As electronics around the world demand more power functionality, and reliability, heat remains one of the major to barriers to achieving maximized performance and to realizing major innovations. Every industry, especially Mobile, Medical, Telecommunications and IoT are developing new applications that are lightweight, multi functional, high power, and required to be more reliable. Engineers are struggling to effectively handle excess heat as consumers demand smaller, thinner, more powerful devices with more options and capabilities.
Two phase cooling is rapidly gaining more popularity in solving these issues. These are technologies are especially ideal for heat spreading for faster dissipation, light weighting, higher reliability and lifetime, but their most significant benefit is design flexibility and the ability to easily integrate them into a system to vastly improve cooling efficiency and capacity. Active air cooling or liquid cooling alone are often too large and cumbersome and come with their own complications such as acoustics, weight, and vibration. By integrating or designing out more active components, two phase can also solve acoustic and vibration issues,
While most engineers are most familiar with heat pipes, which provide the benefits of to phase cooling in a more linear and very flexible for factor, there are several major types of two phase technologies that can handle more heat or feature their own specific benefits and features. Vapor chambers transfer heat in a planar geometry allowing for my uniform heat spreading. Thermosiphons do not require a wicking structure and can be more cost efficient by using gravity to move fluid. Meanwhile, Immersion Cooling is becoming more popular in high power markets as they can work with higher heat loads.
The following guide will touch on each of these technologies and the benefits and considerations when utilizing them to cool your applications.