Liquid Cooling Introduction
Quick Request
What is Liquid Cooling and Why You Should Use It

Liquid cooling is an effective way to remove high heat loads from components. Excessive heat can compromise the reliability of a system and engineers are now turning to liquid cooling when air cooling no longer provides enough heat removal. Two types of liquid cooling are contact cooling and cabinet cooling.
A liquid cooling loop for contact cooling typically consists of a cold plate, pump, heat exchanger, and pipes or hoses. Heat generated by a component is transferred from the component to the thermally conductive cold plate, and then to the liquid coolant that flows through the cold plate. The heated coolant is then pumped through the heat exchanger, where heat is moved from the coolant to either the ambient air or, in the case of a liquid-to-liquid heat exchanger, to another liquid. The cooled liquid then flows through the pipes or hoses back to the cold plate, completing the liquid cooling loop. Instead of a heat exchanger, a recirculating chiller, a liquid cooling system, or facility water may be used to provide cool liquid to the process.
With cabinet cooling the air within the cabinet is cooled by flowing cold liquid through the heat exchanger and distributing the air within the cabinet via the heat exchanger fan. As with contact cooling, cabinet cooling may receive the cold liquid from facility water, a recirculating chiller, or another heat exchanger.
Benefits of Liquid Cooling
Liquid cooling has two primary benefits over air cooling. One benefit is higher performance, since the fluids most commonly used for it have much higher thermal conductivity than air. A second benefit is that it is often much quieter and requires less space than air cooling. Since less air flow is needed, electronics can be packed in more tightly.
Liquid Cooling Technologies
Aavid, Thermal Division of Boyd Corporation designs and manufactures all the thermal components in a liquid cooling loop, providing Total Thermal Solutions. Aavid’s liquid cooling products include both standard and custom cold plates, chassis, chillers, cooling systems, and heat exchangers. Various fluids can be used with the liquid cooling products, including water, deionized water, ethylene glycol, oil, polyalphaolefin, and dielectric fluids. Please contact Aavidto discuss using other fluids.
Liquid Cooling Industry Applications
Liquid cooling is used to cool high power electronic devices within many industries, including medical, military and defense, laser, data centers, semiconductor, transportation, printing, and more.
Liquid Cooling Links
Aavid offers a variety of resources to help you find the right liquid cooling technology for your application. Our liquid cooling application notes are also available in our technical library.
Learn more about our Liquid Cooling Solutions and how you can help cool your system