In product design, thermal solutions typically have a designated volume, called a working envelope. Space: the Final Frontier In the "Project Conditio...
In an earlier blog post, we discuss the importance of user product acceptance. We examined another gaming laptop product review that focused heavily o...
Thermal engineers are radiant about the effects of thermal radiation. Thermal radiation is one of three modes of heat transfer, along with convection ...
In thermal management, we describe our air cooled devices as using either natural convection or forced convection. Fans and blowers are the mech...
We generally take regular events for granted. Sometimes, it's only when our regular programming gets disrupted that we realize how much impact these e...
Thermal Convection: A Pillar of Heat Transfer In a majority of thermal management solutions, we use thermal convection as a means to remove heat away ...
All too often, thermal management is considered too late, if at all, in the design process. In the effort to help make you the thermal expert in your ...
Skived Fin Heat sinks are a single piece construction component for increased surface area and higher heat dissipation. Skived Fin Heat Sinks: Singula...
Heat Sink Bases: a Good Foundation for a Great Solution Heat sink bases facilitate the conduction of thermal energy from heat sources the added surfac...
Thermals affect us everyday, even without us knowing. Heat transfer is just a form of energy transfer. We're busy people and move energy around all th...
Extruded Heat Sinks are a popular choice due to being economical, easy to make in bulk, and require few secondary processes. Extruded heat sinks are o...
As everything becomes more electrified, higher powered, and digitally connected, devices produce more heat that can limit lifetime and reliability of ...
Bonded Fin Heat Sink Assemblies are ideal for high fin:gap aspect ratios that maximizing heat transfer in forced convection solutions. Bonded Fin Heat...
Zipper Fins allow for high fin aspect ratios and more design flexibility due to their progressively stamped construction and assembly. What are Zipper...
An economical option for increasing surface area, folded fins increase heat transfer and performance in heat sinks, heat exchangers, and liquid cold p...
Summer is upon us and it brings some sweltering hot days with it. This is a great time of year to consider your next product and the thermal condition...
Fans and Blowers are a critical tool in air cooled thermal management solutions. Increased flow rate increases heat transfer and dissipation. We're a ...
Brazing generates solid thermal and mechanical joints for fabricating heat sinks, liquid cold plates, heat exchangers, and chassis. What is Brazing? B...
Controlling airflow through a heat sink can generate a large impact on your thermal performance. Ducted Versus Bypass Flow Heat sink performance is im...