Portable Medical Device Case Study
Introduction
Challenge
These devices must be portable, light, easy to use, and affordable while keeping their cooling and operating temperatures at very specific levels for patient comfort and safety. While creating the prototype for their device, Aqueduct Medical sought the expertise of Aavid, Thermal Division of Boyd Corporation, to aid in designing and optimizing the heat dissipation assembly. The prototype had very specific design constraints such as to be easy to use and be unobtrusive in a patient’s home. It also had to be affordable while maintaining proper temperatures to deliver the maximum therapeutic use. Noise, weight, power consumption, and cost all needed to be kept carefully regimented as well as temperature. The industrial design also had to conform well to how the prototype worked and operated.
Solution
Aavid engineered and optimized the heat dissipation assembly for prototyping. The cooling solution was designed with thermoelectric modules placed on a cold plate and an active cooling consisting of heat sinks and a fan while complying with the design constraints of:
• Less than $35 production cost for the cooling solution
• 28℃ Ambient Temperature
• Noise <40dBA at 1m from housing
• Power Supply <220W, 12V DC
Fluid Flow
• Tap water, Distilled water, or Saline.
• Target flow rate < 0.8lpm to enter a liquid cold plate
• Liquid enters the cold plate at a maximum of 7℃
• 60W must be removed from the liquid entering the cold plate
During the design and optimization process, the cost for a mass production version of the cooling solution (heat sink, cold plates) were estimated.
Aavid managed to keep the cost close to the targeted price, the acoustics below the target, and provide a simple, effective and compact cooling solution.
Implementation
The device is used for medical and therapeutic purposes to reduce swelling and ease aches and pains. This can be utilized in both inpatient and in the comport of the users' home. Aavid, Thermal Division of Boyd Corporation designed the cooling solution to make this product work as intended and to the specifications of Aqueduct Medical.
Have questions? We're ready to help!