Thermal Management
Boyd has a long history of developing, designing, testing, optimizing, and fabricating reliable high-performance thermal management solutions across all industries. Through consistent innovation in engineering and manufacturing, Boyd provides optimized, cost-efficient cooling solutions and systems utilizing the largest range of traditional and advanced cooling technologies.
Boyd’s thermal management solutions enable our customers to:
Increase Performance & Functionality
Cooler devices can perform faster, meaning product designers can increase computational processing speed or electronic switching speed to decrease battery charge times or energy conversion.
Reduce Product Size or Create More Design Space
Decrease the weight and volume of a thermal solution for the same device output, leaving room for more functionality or a smaller product.
Extend Product Lifetimes, Improve Reliability, & Product Safety
Excessive heat can wear out materials, including silicon chip processors and lithium ion (Li-Ion) batteries, so keeping your product cool will keep it running longer and safer.
Thermal Management Solutions

Liquid Cooling
Apply the high heat capacity of liquid cooling in liquid systems, chillers, coolant distribution units (CDUs), cold plates, and heat exchangers.

Two Phase Cooling
Spread, transport, and dissipate high heat loads reliably with two-phase vapor chambers, thermosiphon systems, and heat pipe assemblies.

Extreme Air Cooling
Cool your products and systems with cost-effective zipper fin assemblies, extruded heat sinks, or axial fans.

Conduction Cooling
Spread high density heat loads with graphite heat spreaders, encapsulated graphite chassis and enclosures, and thermal interface material.

Sockets
Semiconductor burn-in and test sockets are essential to test and validate all types of integrated circuits

Distribution Partners
Find hundreds of our standard components and thermal solutions for purchase at our Authorized Distributors.

Software
Boyd developed software tools for streamlined and more accurate computational design of complex systems. Since heat pipes, vapor chambers, heat exchangers, and liquid systems are critical cooling solutions, our thermal software solutions allow our engineers to apply them more accurately and have greater confidence in their performance.

Metal Fabrication
Boyd’s broad range of metal additive manufacturing, welding, machining, die casting, brazing, stamping, and finishing enable us to create robust and innovative solutions for structural and thermal management applications.

Tool Room Services
Proper procurement, care, and preservation of your tools is an integral part of improving process performance using fixtures, jigs, and sophisticated robotic automation. Boyd’s dedicated tool procurement team specializes in local and global procurement and implementing preventative maintenance schedules.

Thermal Assemblies
Leverage the breadth of Boyd’s thermal technologies into a single thermal management solution. Boyd’s equipped to manufacture complete liquid systems utilizing liquid cold plates, heat exchangers, tubing, pumps, quick disconnects, and control systems for your high performance cooling requirements. Or utilize ambient air to its’ fullest potential with thermal fans and blowers combined with heat exchangers, thermosiphons, or enhanced heat sinks with heat pipes and vapor chambers.
Metal Fabrication Prototyping Processes
- CNC machining
- Dip brazing
- Friction stir welding
- Internal component machining
- Internal heat pipe fabrication & testing (groove, screen mesh and sintered powder)
- Metal casting
- Metal coating
- Post-processing & finishing
- Sheet metal fabrication
- Vacuum brazing
- Welding (TIG, MIG, plasma, inert gas, braze), including aerospace qualified weld capability
- Soldering and brazing (torch, vacuum, controlled atmosphere)
- Wire EDM (electrical discharge machining)
Thermal Management FAQs
What is thermal management?
Thermal management controls heat in various systems to ensure performance and reliability. It uses solutions like heat sinks, heat pipes, and liquid cooling to prevent overheating and maintain efficiency.What are the basics of thermal management?
Thermal management involves managing heat flow through conduction, convection, or radiation. It uses materials and components like heat sinks, heat spreaders, thermal pastes, and cooling systems to efficiently move and dissipate heat. The goal is to balance heat generation with dissipation to keep systems running reliably.What is the thermal management system?
A thermal management system controls heat by using components like heat sinks, fans, liquid cooling, and thermal interface materials to regulate temperature. It ensures systems run efficiently and reliably by preventing overheating.What are thermal management strategies?
Thermal management strategies include passive and active cooling methods to control heat. Passive strategies rely on natural heat dissipation using heat sinks and thermal spreaders. Active strategies employ fans, pumps, and refrigeration systems to enhance heat removal. Optimizing airflow, using thermal interface materials, and integrating phase change materials also improve thermal performance.How do you calculate thermal management?
To calculate thermal management, assess the heat generated by components and the required cooling capacity. Begin by determining the thermal resistance of materials and calculate heat transfer using conduction, convection, and radiation formulas. Factor in ambient temperature and desired operating temperatures to ensure efficient heat dissipation. Use this data to select effective thermal management solutions that meet performance requirements.What is the basic thermal process?
The basic thermal process involves transferring heat through conduction, convection, and radiation. Conduction transfers heat through solid materials, convection moves heat through fluids, and radiation transfers heat through electromagnetic waves. Together, these processes regulate temperature and maintain efficient thermal management in systems.What are the different types of thermal control?
Thermal control includes active cooling, passive cooling, and thermal insulation. Active cooling systems, such as fans and refrigeration units, remove heat from components. Passive cooling relies on natural heat dissipation using materials like heat sinks and thermal spreaders. Thermal insulation minimizes heat transfer, protecting sensitive components from temperature fluctuations. Each type plays a vital role in maintaining optimal operating conditions for various applications.What is thermal management in space?
Thermal management in space controls temperatures of spacecraft and satellite systems to ensure optimal performance in extreme environments. It employs insulation, radiators, and active thermal control systems to manage heat from onboard equipment and solar radiation. Effective thermal management prevents overheating and ensures reliable operation of sensitive components throughout the mission.Have questions? We’re ready to help!