1 minute reading time (210 words)

Advantages & Disadvantages of Standardizing O-Rings

O-Ring Size has standardized over time to simplify design and manufacturing, but may not always be the best solution for every application.

Standardization of O-Ring Sizes

When the O-Ring concept was originally developed, there was no standardization of sizes. Product designers and manufacturers would design O-ring seals specifically for their applications and machinery, meaning O-Ring suppliers would only produce specific sizes they had customers for. Very few sizes, if any, were used by more than one customer and this lack of standardization discouraged O-Ring manufacturers from producing in the most economical quantities.

The United States government recognized the commercial need for standardized O-Ring sizes and developed the aerospace size standard chart (AS568). The AS568 size chart identifies standard sizing by inside diameter and cross-sectional thickness, with reference dimensions for outside diameter. Other standard size charts include British Standard (BS), European standard, and Japanese standard.

Related Products and Resources

Surface Energy and Adhesive Selection
How Hot is too Hot? The Real Maximum Temperature o...

Related Posts