Home » Blog » Glass Printing Techniques

Glass Printing Techniques

From screen printing to digital printing to frit printing, there are several techniques used at Boyd to print on glass.

To ensure the success of any glass-printing application, there are numerous factors that go under consideration such as glass type, inherent tint of the glass, ink type, ink color, curing process, and environmental conditions. However, one crucial factor that needs to be determined is the print method. Glass can be printed on using one of the three techniques: screen printing, digital printing, or frit printing. While all these methods support different shapes, sizes, thicknesses, types of glasses, and allow the use of multiple colors, there are unique pros and cons that distinguish them.

Screen Printing on Glass

The first step is to specifically define what the device will be used for, as this can dictate which touchscreens are feasible. For instance, will your display be used for a military application where it may be subject to harsh conditions, or is the screen intended for an inexpensive toy where durability may not be a huge concern? Both situations would require screen technologies with different functionality, durability, input registration, and pricing. Once you’ve narrowed down the intended use for the display, the next step is to figure out which functionalities are necessary.

Digital Printing on Glass

Digital printing on glass functions like a regular inkjet printer, where the only requirement is digital art file to print. It affords greater flexibility in terms of changing designs at the last minute. Unlike screen printing, where any design variation requires the construction of a new screen, modifying an art file for digital printing is quick and easy. This makes it a great choice for prototyping and achieving faster time-to-market products. But it is important to note that the inks utilized for glass digital printing are thinner compared to the inks employed in screen printing. Hence, while working with light or pastel shades, multiple layers may be required to achieve a sufficient level of opacity. This can lead to an increased thickness and can pose challenges in the optical bonding process. In contrast to screen printing, where one color is printed at a time, digital printing also allows the printing of all the different colors at once. Digital printing on glass is currently undergoing continuous developments to accommodate more types of inks.

Frit Printing on Glass

Frit printing is similar to screen printing with the exception of the ink utilized and the curing process. A unique powdered-glass ink is screen printed onto the glass and cured during the heat tempering process. The heat fuses the ink to the glass, offering strong adhesion and making it difficult to remove or scratch the ink off. Since frit printing offers the highest durability out of all the techniques, it’s ideal for applications where the glass is regularly exposed to challenging environmental conditions commonly found in the defense, industrial, and eMobility sectors. However, it is also the most expensive printing method and therefore, not as frequently employed. While frit printing can be done on heat-tempered glass, it generally cannot be utilized for chemically-strengthened glass, as the glass thickness has to be greater than 2mm for the frit printing process. Frit colors are also limited to black, white, and some grays.

Bringing together the right mix of functionality and durability for your custom application, the experts at Boyd can not only help you select the most suitable printing technique for your glass application, but also support your glass printing and bonding needs from prototyping through production. To learn more about Boyd’s bonding solutions, schedule a consultation with our experts.