Blog, Liquid Cooling, Thermal
In many liquid cooling loops, the heat that is picked up by a cold plate is rejected to ambient air via a heat exchanger. Calculating the Thermal Resistance of a Heat Exchanger Figure 1 shows a typical liquid cooling loop, consisting of a cold plate (CP), pump, and...
Blog, Liquid Cooling, Thermal
Heat exchanger prices can vary quite a bit; understanding why can help you cut costs and still obtain the performance you need to properly cool your application. Key Factors that Determine the Cost of Fabricating Heat Exchangers Manufacturing costs can be greatly...
Air Cooling, Blog, Liquid Cooling, Thermal
A heat exchanger is a device designed to efficiently transfer or “exchange” heat from one matter to another. When a fluid is used to transfer heat, the fluid could be a liquid, such as water or oil, or could be moving air. How to Calculate Which Fan is...
Air Cooling, Blog, Liquid Cooling, Thermal
In order to select the correct heat exchanger or oil cooler, you must first determine required thermal performance for your application. Use the example shown below: Select the Cooling Liquid Step 1: Application Data Liquid Type: Water Required Heat Load (Q): 3,300 W...
Blog, Liquid Cooling, Thermal
Fluid line connectors are essential to liquid cooling loops. Engineers must consider selection, installation, and maintenance of a system’s fluid connections to prevent leaks and ensure system longevity. Fluid Coupling and Connector Selection Choosing the Right...