Solar Team Twente Case Study
Project Details
Customer: Solar Team Twente
Application: Solar Car Engine
Technology: Brazed Fin
Industry: Research / Green Energy
Location: Twente, Netherlands
Challenge
In May of 2015 Aavid, Thermal division of Boyd Corporation, in Bologna,Italy received an urgent request from our favorite student racing team -Solar Team Twente from the University of Twente. They had designed, built and tested an amazing solar car with one andonly ambition: win the World Solar Challenge 2015 driving across theAustralian Desert. In 2012 Aavid had developed a cooling solution fortheir solar-powered control electronics. Now they needed a radicalweight reduction to help improve the solar car’s performance. Timing was short. To make the race qualification deadline, we needed toconceptualize, analyze, build, test and deliver prototype cooling solutionsin just a few weeks. Working closely with Solar Team Twente, that isexactly what we did.
Solution
The existing solution used by the team was developed by Aavid in Bologna, Italy in 2012. It was constructed from formed aluminum fins brazed to a baseplate. During the tests for the competition in 2013, the team observed that in operation the heatsink was “too cold to be true”. At a weight of 0.74 kg (1.6 pounds), the cooling solution was clearly oversized, overweight and over performing for the latest reduced heat load.
We needed to very quickly re-optimize the design for minimum weight while maintaining adequate thermal performance. Analysis showed that we could significantly reduce the fin height and pitch. The team decided to stick with the brazed assembly process, so the base and fin thicknesses were set at the minimums required for brazing.
Modeling predicted that Aavid could to reduce the weight of the thermal solution by 50% reaching 0.36 kg (0.8 pounds) while meeting the thermal requirements. Aavid rapidly formed the fins, used CNC to machine the base, brazed together the entire structure, sand-blasted it, and applied a black anodize finish to enhance radiated transfer.
Solar Team Twente completed the test and the results were exactly as Aavid predicted - great thermal performance at half the weight. Best of luck to Solar Team Twente in Australia!
Have questions? We're ready to help!