Right Sizing Liquid Components and Systems

The Benefits of "Right-Sizing" Components & Systems Designers sometimes oversize components in order to build in a margin of safety. However, this...

Continue reading

Regenerative Turbine Pump Maintenance

The following is a brief overview of some fundamental heat transfer concepts. To learn more, the reader is encouraged to review the source publication...

Continue reading

Reducing Contact Thermal Resistance

The trend in the electronics packaging industry is towards smaller, more powerful devices. With these small, high power components, however, there are...

Continue reading

How to Measure your Heat Load

Formula for Specific Heat The first step in selecting the proper product for your cooling system application is to determine the heat load, or the amo...

Continue reading

Fundamentals of Heat Transfer

The following is a brief overview of some fundamental heat transfer concepts. To learn more, the reader is encouraged to review the source publication...

Continue reading

Defining Heat Source’s Dissipated Power

Input Power versus Dissipated Power For those new to thermal management, most devices have two associated power values: input power and dissipated pow...

Continue reading

The Basics of Heat Transfer

Heat Spreading Heat spreaders offer cost-effective, reliable high thermal conductivity and efficacy with almost no moving parts. A heat spreader is an...

Continue reading

How to Calculate Maximum Case Temperature of a Device

Gathering Critical Device Data Finding how much heat your electronic device dissipates and how to calculate maximum case temperature can be difficult ...

Continue reading

The Basics of Compressor-Based Refrigeration

When trying to understand how a compressor based cooling system works, you must keep three physical phenomena in mind: Fundamental Physical Principles...

Continue reading

Frequently Asked Thermal Questions

Get answers to frequently asked questions about heat pipes, thermal technology and thermal management. Heat Pipes and Heat Exchangers What is a heat p...

Continue reading

Laser Liquid Cooling Optimization

The performance of high-powered lasers depends on effective cooling. High-powered lasers generate a significant amount of heat that must be removed fr...

Continue reading

High Performance Liquid Cooling Loop Design

Embedded systems are becoming more complex, processing and analyzing a growing number of sensors and signals. The result of this increased computing i...

Continue reading

Liquid Cooling Introduction

Liquid cooling is an effective way to remove high heat loads from components. Excessive heat can compromise the reliability of a system and engineers ...

Continue reading

Selecting a Liquid Cooling System

Ambient cooling systems, recirculating chillers, liquid-to-liquid cooling systems there are so many different cooling technologies that selecting...

Continue reading

Assessing the Quality of a Tubed Cold Plate

As many applications move from air cooling to liquid cooling, tubed cold plates are often a cost efficient and popular solution. Although many local s...

Continue reading

Liquid Cold Plate Manufacturing Cost Drivers

Liquid cold plate prices can vary quite a bit; understanding why can help you cut costs and still obtain the performance you need to properly cool you...

Continue reading

Designing Custom Liquid Cold Plates

Liquid-cooled cold plates offer superior cooling for high power electronic devices and can be purchased as standard products or can be custom designed...

Continue reading

Selecting a Liquid Cold Plate Technology

Complex systems that utilize liquid flow rely on leak-free systems, dependable liquid containment, transport, and sealing solutions. These active syst...

Continue reading

Sizing a Heat Exchanger for Cold Plate Applications

In many liquid cooling loops, the heat that is picked up by a cold plate is rejected to ambient air via a heat exchanger. Calculating the Thermal Resi...

Continue reading

Heat Exchanger Manufacturing Cost Drivers

Heat exchanger prices can vary quite a bit; understanding why can help you cut costs and still obtain the performance you need to properly cool your a...

Continue reading

Selecting a Heat Exchanger

In order to select the correct heat exchanger or oil cooler, you must first determine required thermal performance for your application. Use the examp...

Continue reading

Introduction to Pressure Drop

Thermal interface material (TIM) is a crucial part of any thermal management solution. Since it's physically a small portion of most applications, it'...

Continue reading

Couplers, Hose Clamps and Fitting Selection

Fluid line connectors are essential to liquid cooling loops. Engineers must consider selection, installation, and maintenance of a system's fluid conn...

Continue reading

How Thermal Interface Material Works

Thermal interface material (TIM) is a crucial part of any thermal management solution. Since it's physically a small portion of most applications, it'...

Continue reading

Avoiding Corrosion in Liquid Cooling Systems

Water and water/glycol solutions are common heat transfer fluids used in cooling systems and recirculating chillers. Although the fluids are the lifeb...

Continue reading

Liquid Cooling System Pump Overview

Complex systems that utilize liquid flow rely on leak-free systems, dependable liquid containment, transport, and sealing solutions. These active syst...

Continue reading

The Best Heat Transfer Fluids for Liquid Cooling

Once you've determined liquid cooling is the solution, do you know what heat transfer fluid to use? One of the most important factors when choosing a ...

Continue reading

Recirculating Chiller Protection Options and Fluid Compatibility

Recirculating chillers are "off-the-shelf" liquid cooling systems that offer precise temperature control and/or cooling below ambient temperatures. Ex...

Continue reading

Chiller Temperature Control

Industrial chillers are commonly used to circulate a constant temperature fluid in a closed loop with liquid cooled instruments and tools in order to ...

Continue reading

Recirculating Chiller Maintenance

Recirculating chillers are cooling systems that provide precise temperature control as well as cooling below ambient temperature. Key Preventative Mea...

Continue reading

Selecting a Recirculating Chiller & Cooling Capacity Factors

Selecting the proper recirculating chiller is a function of four factors: The heat load generated by the device being cooled (Q)The maximum acceptable...

Continue reading

Heat Exchanger Fan Selection

A heat exchanger is a device designed to efficiently transfer or "exchange" heat from one matter to another. When a fluid is used to transfer heat, th...

Continue reading

Introduction to Thermal Management: Keeping Devices Cool

The latest electrification trends drive products to contain more powerful and compact electrical components, which drives additional thermal managemen...

Continue reading

Thermal Management in Artificial Intelligence

As technology continues to evolve, more companies leverage Artificial Intelligence (AI) to improve existing offerings and generate new solutions to ac...

Continue reading