The SuperCam Instrument Suite on the NASA Mars 2020 Rover: Body Unit and Combined System Tests



Boyd Develops Cooling Solution for the Critical SuperCam Assembly of the Perseverance Mars Rover



As NASA prepares for the launch of the Perseverance Rover, planned for July 22nd, 2020, Boyd Corporation is proud to highlight our contribution to the next stage of Mars exploration, developed in collaboration with Los Alamos National Laboratory. Overcoming harsh environments when exploring another planet challenges even the best engineering teams to ensure electronics can and continually operate in varying and unfamiliar conditions. Preparing to explore the Martian surface required creativity, determination, innovation, and perseverance.



The SuperCam Module of the Perseverance Mars Rover



NASA’s Perseverance Rover mission is to search for signs of previously or currently habitable conditions on Mars and for signs of past microbial life. The SuperCam utilizes remote-sensing techniques to conduct minerology analysis of both the environment and samples within the robotic-arm workspace. The SuperCam is a technological improvement over Curiosity’s ChemCam, as it adds two new techniques for determining mineralogy a color imager, and an acoustic system to remotely determine physical properties of targets.

The SuperCam includes a broad range of spectroscopy instruments, some of which utilize Thermal Electric Coolers (TECs) that use the Peltier effect to pump heat away from electronics and maintain tight temperature control. The TECs need to reject heat to help protect the electronics vital to minerology observations.

Credits: NASA/JPL-Caltech



February 07, 2020 The Mast Unit for Mars 2020's SuperCam, shown being tested here, will use a laser to vaporize and study rock material on the Red Planet's surface.



Custom Cryogenic Heat Pipes to Withstand Martian Environments



Heat pipes are a common component in many electronic assemblies used to either spread or transport heat. Many applications use heat pipes to prevent heat build-up and potential damage to sensitive and expensive equipment by quickly moving heat away to cooler regions. While most heat pipes are robust and straightforward; customizations and material selections enable these straightforward solutions to solve more complex challenges, applications and operating environments.

For the Perseverance Rover, maintaining a safe operating temperature of data collection equipment is paramount to the success of the rover. There is no way to do maintenance and repair to the Rover once it’s launched, so thermal management solutions must reliably perform in extreme temperatures common on Mars over the entire lifetime of the rover. Failure is not an option. Boyd’s heat pipes are an ideal solution for space applications like these as they’ve been proven to operate consistently over decades of operation with no active moving parts.

Mars is much colder than Earth but there is less atmosphere, so natural convection air cooling is much slower making electronics at risk of overheating despite the colder environment. This colder environment makes common copper-water heat pipes unsuitable for the Mars Rovers. To solve the performance and environment challenge, Boyd uses our Material Engineering expertise to feature methanol as an alternative working fluid for passive two-phase cooling, which doesn’t freeze at Rover temperatures.

Boyd has previous experience fabricating solutions for Mars missions, making us a solid partner in developing reliable thermal management solutions that meet the demands of reliably performing on Mars. We leveraged our understanding of Martian environment design challenges to create a new heat pipe solution in partnership with Los Alamos National Labs for the SuperCam module. The SuperCam module enables critical imaging, mineral, and chemical analysis, a central portion of the Perseverance Rover mission.

Los Alamos National Labs approached Boyd to help transport a total 6W of heat away from the charge-coupled devices (CCDs, optical detectors) within the SuperCam Module to be transferred to thermoelectric coolers (TECs). As a team, LANL and Boyd developed three heat pipe assemblies to cool 2W each, constructed with two 5mm diameter plated copper-methanol heat pipes. This enables a stable ~20°C of cooling below the temperature of the Rover Accessory Mounting Plate (RAMP).*

Los Alamos National Labs- NASA Super Cam Assembly with Boyd Corp. Heat Pipes



July 02, 2019 Engineers install the SuperCam instrument on Mars 2020's rover. This image was taken on June 25, 2019, in the Spacecraft Assembly Facility at NASA's Jet Propulsion Laboratory, Pasadena, California



One Company, Many Solutions for Space Exploration



Thermal Management is only one of Boyd’s strengths when it comes to supporting space exploration and aerospace applications. From our flame-resistant SOLIMIDE® Insulating Foams to EMI/RFI Management, Boyd can help protect your equipment and cargo in the demanding environments of space with thin atmospheric conditions. Other Engineered Material solutions like Optically Clear Adhesives and High Performance Gaskets protect camera and sensor lenses, sealing and protecting against harsh external environments.

Boyd strives to provide quality, reliable solutions to all industries, but it is a privilege to support the Perseverance Rover and be a part of NASA’s mission to explore Mars. Our long tradition of providing highly engineered thermal management solutions for space exploration will enable the Perseverance Rover to endure for years to come.



Preparing for Launch



As NASA is making final preparations for the launch, Boyd Corporation continues to develop and fabricate solutions for upcoming Martian projects. We’re looking forward to a successful launch on July 22nd (or August 11th at the latest) and the eventual deployment of the Perseverance Rover on Mars in February 2021. Good Luck NASA and thank you Los Alamos National Laboratory for the opportunity to be a part of history!