The term "centrifugal pump" encompasses a multitude of pump technologies. Centrifugal means "directed or moving away from a center or axis", therefore a centrifugal pump uses a rotating impeller to move the fluid outward. Fluid enters the pump and is drawn into the eye, or center, of the impeller and then is forced outward through the vanes (blades) via centrifugal force generated by the rotating action of the impeller. The fluid is forced to the outside of the pump casing (or volute) and out the pump's discharge (see figure 1). The flow of a centrifugal pump depends on the system pressure drop: the higher the pressure drop, the lower the flow.
Many of Boyd’s liquid cooling systems use seal-less, magnetically-driven centrifugal pumps, also known as mag-drives. Magnetically driven pumps use two magnets to drive the impeller. One magnet is attached to the motor shaft, generally referred to as the "drive magnet". The other magnet is attached to the impeller (the "driven" or "impeller" magnet). The drive magnet spins causing the impeller magnet, and therefore impeller, to spin at the same rate. This pump design eliminates pump seals which often wear out from the friction caused by the rotation of the motor shaft and are a source of leakage. In our centrifugal pumps, the drive magnet is integrally molded into the impeller and thermoplastically coated to ensure zero contamination of the pump fluid. Thus, "mag-drive" ensures pump integrity and eliminates any possibility of shaft or seal leakage.