Infineon Technologies has partnered with Boyd Corporation to develop improved systems and solutions for cooling electronics in hybrid and electric vehicles (HEV/EV). Production and consumer adoption of these vehicles are expected to grow exponentially over the next 20 years as the need for cleaner, more compact, less expensive transportation increases to meet environmental standards.
In addition to new power and energy requirements, customer demands also require greater connectivity and more powerful internal electronics and vehicle operating systems. The growing need for new technologies and better performing electronics ultimately results in an excess of heat. Without proper thermal management, the reliability and lifetime of electronics necessary to keep these vehicles running safely is significantly impaired to the point of device and system failure.
The partnership between Infineon and Boyd enables our teams to jointly design and produce fully optimized, highly effective cooling solutions for Infineon’s high performance electronics for eMobility and Hybrids.